cancel
Showing results for 
Search instead for 
Did you mean: 

SPI1 DMA channel/stream

russdx
Associate II
Posted on October 25, 2012 at 14:38

Where do I find out what DMA channel/stream i need to use for SPI1 TX.

not sure which st document has this information in it?

(stm32f4)

Thanks :)
2 REPLIES 2
Posted on October 25, 2012 at 17:12

The RM0090 Reference Manual

DMA2 request mapping table (Table 21, Pg 165 in Rev 1)

SPI1_TX DMA2 Channel 3, Stream 3 or Stream 5

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
russdx
Associate II
Posted on October 25, 2012 at 17:57

perfect :)

Thanks