cancel
Showing results for 
Search instead for 
Did you mean: 

SPI with non standard clk cycles.

Andrew C
Associate III

Is there a way to have spi just send an abnormal number of clock cycles as opposed to just 8 cycles at a time? Is bit banging the only way? Can the LL library be configured or coded to do such a thing?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

Some newer STM32 allow anyting between 4 and 16 bits.

JW

S.Ma
Principal

Yep, actually played with it for fun to try to generate SWD type bitstreams joggling with 8, 6 and 9 bits.

You can choose chunks of 4 to 16 bit. As long as the chunk size is the same, you can poll the FIFO TX level to preload next chunk without delays in transmission which will be only needed when you change gears (bit size)

PBU
Associate III

Hi,

I am using HAL Library. I need to send 9 bits using SPI. I have configure the SPI with 9 bit data length. While sending the 9 bit data were clocked out for the first time alone, if i transfer second time it had clock out 8 bits only. Give me a suggestion to solve this issue.

Thanks