SPI Transmit only last word of byffer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 7:54 AM
Hi
I'm trying to transmit 4 16-bit words via SPI as slave using interrupts and HAL.
I'm using STM32F107VCT6
So I specified a buffer:
uint16_t buf[] = {0x000F, 0x00F0, 0x0F00, 0x0004};And started to transmit in main:
MX_SPI2_Init();
HAL_SPI_Transmit_IT(&hspi2, (uint8_t *)buf, 4);
while (1)
{
//some logic
}Spi was initialized with CubeMX:
static void MX_SPI2_Init(void)
{
/* USER CODE BEGIN SPI2_Init 0 */
/* USER CODE END SPI2_Init 0 */
/* USER CODE BEGIN SPI2_Init 1 */
/* USER CODE END SPI2_Init 1 */
/* SPI2 parameter configuration*/
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_16BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_HARD_INPUT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI2_Init 2 */
/* USER CODE END SPI2_Init 2 */
}That is what I get:
What am I doing wrong?
- Labels:
-
SPI
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 8:15 AM
Your code sends the 4 halfwords ONCE.
Is the LA picture you posted the FIRST transaction after the slave has been reset?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 8:39 AM
Thanks for the answer!
You are right, first transaction is correct.
What is the correct way to transmit data "by request" using interrupts?
Is there any way to get interrupt by hardware NSS?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-12 8:59 AM
>What is the correct way
There's no "one correct way", it depends on your application.
> Is there any way to get interrupt by hardware NSS?
Use EXTI interrupt - Cube will get into your way. It's a recurring theme her, search, there's among others also a quote recent related thread.
JW