2015-09-21 7:52 AM
Hello,
I use a stm32f103, I want to use the SPI peripheral in slave mode.The SPI Master is configured with a clock at 1Mhz.I must to configure the STM32 SPI peripheral with a clock at 1Mhz, but its not possible with these prescalers availables, I can have 1.5Mhz or 0.75MKhz.Which clock I must choose ? the upper or the lower ?Thanks :) #spi-slave-mode #spi-stm32f1032015-09-21 8:28 AM
Pretty sure the slave shouldn't care, it's using the master's clock to shift the data, and the peripheral is clocking at the APB rate internally.