Question
SPI protocol STM32F303
Posted on April 04, 2015 at 08:49
Hi,
I am a newbie in the field of micro-controllers and I'm having trouble programming the GPIOA parts as SPI1. Could someone please tell me where I could be going wrong? I would greatly appreciate if someone points me towards SPI implementation examples. The routines I've written so far are given below. I am trying to send just a byte of data and I am using a logic analyzer to check if there's a clock on SCK pin but I don't see anything happen. I also tried toggling an LED by sending data continuously but even this fails. void spi_initialization(void){ SPI_I2S_DeInit(SPI1); SPI_InitStructure.SPI_Direction= SPI_Direction_1Line_Tx; SPI_InitStructure.SPI_Mode= SPI_Mode_Master; SPI_InitStructure.SPI_DataSize= SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL=SPI_CPHA_2Edge; SPI_InitStructure.SPI_CPHA= SPI_CPOL_High; SPI_InitStructure.SPI_NSS=SPI_NSS_Soft ; SPI_InitStructure.SPI_BaudRatePrescaler=SPI_BaudRatePrescaler_2; SPI_InitStructure.SPI_FirstBit=SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial=7; SPI_Init(SPI1,&SPI_InitStructure); SPI_RxFIFOThresholdConfig(SPI1, SPI_RxFIFOThreshold_QF); /* Enable SPI1 CRC calculation */ SPI_CalculateCRC(SPI1, ENABLE); //SPI_BiDirectionalLineConfig(SPI1, SPI_Direction_Tx); SPI_Cmd(SPI1, ENABLE); }void send_byte(uint8_t val){ GPIO_ResetBits(GPIOA, GPIO_Pin_4); // CS low while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET); //wait buffer empty SPI_SendData8(SPI1, val); while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET); //wait finish sending GPIO_SetBits(GPIOA, GPIO_Pin_4); // CS high}void RCC_config(){ //System clock set as HSI RCC_SYSCLKConfig(RCC_SYSCLKSource_HSI); // clock freq is 4MHz RCC_HCLKConfig(RCC_SYSCLK_Div2); // CLock freq divided by 2 to get 2MHz again on APB2 peripherals for SPI1 //RCC_PCLK2Config(RCC_HCLK_Div1); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);}void GPIO_config(){ // Setting the pins for alternate mode SPI configura MOSI, SS, SCK //GPIO_PinAFConfig(GPIOA, GPIO_PinSource4|GPIO_PinSource5|GPIO_PinSource7, GPIO_AF_5); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); // Set GPIO pin for reset of LCD GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOE, &GPIO_InitStructure); // Set GPIO pin as NO PULL for RS functionality GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStructure); }int main(void){ // Initialize clocks RCC_config(); GPIO_config(); spi_initialization(); send_byte(0xFF);} #spi-protocol-stm32f303