2015-10-15 4:27 AM
Hi ,
I have an SPI program running successfully between two stm32f4 discovery boards using SPI_NSS as SPI_NSS_Soft. Some discussions on Stm32f4 SPI say that SPI_NSS_Soft has to be used when only one slave. Does that mean that when only 1 slave , we are not allowed to use SPI_NSS_Hard ? But if we can use SPI_NSS_Hard then , what would be the difference in the configuration of the pins for sck , miso , mosi and nss on the master and on the slave side? Thank you so much. #stm32f4 #discovery #spi #device2015-10-15 5:08 AM
NSS_Hard implies to use one extra pin on both mcu. Do you want to spend a pin unnecessarily?
JW2015-10-15 5:21 AM
Hi,
Thank you for replying . Yes you are right. It makes no sense to waste a pin. But was just curious to if with only one slave NSS_Hard could be used. Thank you!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.