Question
SPI Master Read Write using HAL commands
Posted on March 31, 2017 at 04:56
Hi All,
I am new to STM , I have problem in read and write data simultaneously using STM32L476 board. i just created a new project using STMcubeMX and try to read and write simultaneously using HAL_SPI_TransmitReceive_IT , and when i checked on my spi sniffer, spi data is sent byte ,byte ... Here my spi init config
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT ; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 7; hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;if (HAL_SPI_Init(&hspi1) != HAL_OK)
is any missing in my configuration.
Thanks in advance.