cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Issues: NSS stays low, clk pol high toggling

Steven Keeter
Associate III
Posted on April 12, 2018 at 18:46

Using STM32F0 device and having some trouble with NSS hard output returning high after transaction, and also when using idle high clock polarity the preamble idle state is changing.  Sometimes it toggles high before start, other times it remains high until start.  I've seen comments about pull-up setting used on these pins and also seen comments on having to call De-Init after each spi transfer.  Seems the hardware should handle these???  When using NSS soft control the toggling of the clock polarity before spi transaction start seems problematic.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on April 12, 2018 at 19:37

Please edit so the entire question isn't in the Summary/Title field, thanks.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..