2013-11-21 8:52 AM
Hi,
I am using SPI2 with DMA1 on STM32F427 to communicate with an external processor. The problem is that when the data on MISO and MOSI pins (PB14 and PB15) are somehow corrupted i.e. the data comes out as shifted versions of the data sent and the amount of the shift always changes and same thing goes for also the receive part; received data is the shifted version of the data in the input pin. What might be the cause of this problem? Could some other functions of the pins be interfering my application?2013-11-21 8:58 AM
There is no intrinsic framing, so figure if your clock is getting noise or being missed. Look at how you are driving it, how it is being terminated, the edges and the speed.
Try it slower. Make sure you have good common grounds. Use a logic analyzer and understand why and when you are losing bit synchronization/framing. Consider if you can use CS for bit/byte framing.2013-11-22 12:01 AM
Hi Clive,
I tried the same code using STM32F4 discovery board and configured SPI2 as master with DMA1. I observed the output data with scope and saw that the bits are still shifting. I think this shows that my problem is not related with hardware or noise. Do you think it could be software related; may be about burst sizes? I am also sending my code below. SPI_InitTypeDef SPI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure;DMA_InitTypeDef DMA_InitStructure;NVIC_InitTypeDef NVIC_InitStructure;RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE);GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2); // SCKGPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2); // MISOGPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2); // MOSI//Configure the pins used for SPIGPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;GPIO_Init(GPIOB, &GPIO_InitStructure);SPI_I2S_DeInit(SPI2);SPI_StructInit(&SPI_InitStructure); // SPI configurationSPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;SPI_InitStructure.SPI_CRCPolynomial = 7;SPI_Init(SPI2, &SPI_InitStructure); SPI_Cmd(SPI2, ENABLE); /*********************************************************************************************/// DMA for TxDMA_DeInit(DMA1_Stream4); DMA_StructInit(&DMA_InitStructure); DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) & (SPI2->DR); DMA_InitStructure.DMA_Channel = DMA_Channel_0; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral; DMA_InitStructure.DMA_Memory0BaseAddr =(uint32_t) &Tx_Buffer_to_AP1; DMA_InitStructure.DMA_BufferSize = 4096; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_DoubleBufferModeConfig (DMA1_Stream4 ,(uint32_t) &Tx_Buffer_to_AP2, DMA_Memory_0);DMA_DoubleBufferModeCmd(DMA1_Stream4 , ENABLE); DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;DMA_Init(DMA1_Stream4 , &DMA_InitStructure); /************************************************************************************/// DMA for RxDMA_DeInit(DMA1_Stream3); DMA_StructInit(&DMA_InitStructure);DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) & (SPI2->DR); DMA_InitStructure.DMA_Channel = DMA_Channel_0;DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory ; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t) &Rx_Buffer_from_AP;DMA_InitStructure.DMA_BufferSize = 4096; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;DMA_Init(DMA1_Stream3 , &DMA_InitStructure); /***************************************************************************************/NVIC_InitStructure.NVIC_IRQChannel = DMA1_Stream4_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_Init(&NVIC_InitStructure);NVIC_InitStructure.NVIC_IRQChannel = DMA1_Stream3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_Init(&NVIC_InitStructure);DMA_ITConfig(DMA1_Stream3, DMA_IT_TC, ENABLE); DMA_ITConfig(DMA1_Stream4, DMA_IT_TC, ENABLE);SPI_I2S_DMACmd(SPI2, SPI_I2S_DMAReq_Tx, ENABLE); SPI_I2S_DMACmd(SPI2, SPI_I2S_DMAReq_Rx, ENABLE);2013-11-22 1:24 AM
SPI is not a ''standardized'' protocol, so you will need to check if the master and slave settings do match. One of those subtle items is the CLK pulse transition which triggers the read. If that doesn't match, you will have random effects.
I would re-check the datasheets.2013-11-22 7:41 AM
I observed the output data with scope and saw that the bits are still shifting.
I'm having a hard time visualizing this, can you post a screen plot of the Clock and Data signals that illustrates this? The code is missing some critical context, can you perhaps NOT use DoubleBuffer mode, and try using a single double sized buffer with HT/TC?