2018-01-11 04:29 AM
Hi,
I am using STM32L4 MCU. Facing a problem with SPI communication.
MCU clock:48Mhz
SPI clock enabled as 6Mhz
Using a interrupt for SPI write.
I am seeing 17us time duration (3us clock + 14ms idle time) between a bytes transfer (I have probed the clock line using scope). so that throughput is reducing for data read for my application.
1) why in between two clock frame 14us delay?
2) how can i reduce the delay between bytes transfer?
#spi-delay-between-bytes-write...2018-08-10 09:29 AM
Sorry, bumping old zombie unanswered threads off my feed