2021-06-25 1:11 AM
I configured my spi to have a datasize of 8bits. However, its sending an extra '\0' after every letter and i can't figure out where this is coming from. Am running a Nucleo-F303k8.
Here below, am trying to send a Hello World! message but it gets corrupted all the way.
Here is how i configured my settings.
void SystemClock_Config(void);
void SPIConfig(void)
{
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; // Enable SPI1 Clock
SPI1->CR1 |= SPI_CR1_CPHA | SPI_CR1_CPOL; // Enable CPHA=1 and CPOL=1
SPI1->CR1 |= SPI_CR1_MSTR; // Master Mode
SPI1->CR1 |= (7 << 3); // Baudrate divide with 256
SPI1->CR1 &= ~(SPI_CR1_LSBFIRST); // LSBFIRST = 0, MSB_FIRST = 1
SPI1->CR1 |= SPI_CR1_SSM | SPI_CR1_SSI; // SSM = 1, SSI = 1 -> Slave Management
SPI1->CR1 &= ~(SPI_CR1_RXONLY); // Full-duplex (Transmit and receive)
SPI1->CR2 |= (7 << 8); // SPI Datasize -> 0111: 8-bit
__IO uint32_t tempRD = SPI1->SR; // Clear all flags in the status register
}
void GPIOConfig(void)
{
RCC->AHBENR |= RCC_AHBENR_GPIOAEN; // Enable GPIOA
// b10: Alternate function mode for PINS MOSI, SCLK & MISO
GPIOA->MODER |= (2 << 14 | 2 << 10 | 2 << 12);
// General purpose output mode for CSN PIN
GPIOA->MODER |= (1 << 8);
// b11: High speed for all 4 pins
GPIOA->OSPEEDR |= (3 << 14) | (3 << 12) | (3 << 10) | (3 << 8);
// Set to alternate function AF5 which corresponds to SPI1
GPIOA->AFR[0] |= (5 << 28) | (5 << 24) | (5 << 20);
// GPIO port pull-up/pull-down register
GPIOA->PUPDR &= ~(1 << 14 | 1 << 12 | 1 << 10 | 1 << 8);
// Put the output type of CSN pin to output push-pull ( reset state)
GPIOA->OTYPER &= ~(1 << 4);
// Set the CSN ODR to High initially
GPIOA->ODR |= (1 << 4);
}
// SPE = 1, peripheral enabled
void SPI_Enable(void)
{
SPI1->CR1 |= SPI_CR1_SPE;
}
// SPE = 0, peripheral disabled
void SPI_Disable(void)
{
SPI1->CR1 &= ~SPI_CR1_SPE;
}
void CSN_Enable(void)
{
GPIOA->ODR &= ~(1 << 4);
}
void CSN_Disable(void)
{
GPIOA->ODR |= (1 << 4);
}
void SPI_Transmit(char *data, int size)
{
uint8_t i = 0;
while(i < size)
{
// Wait for TXE bit to set -> This indicactes that the buffer is empty and ready to recieve stuff
while(!(SPI1->SR & SPI_SR_TXE)) {};
// Load data into the data register
SPI1->DR = data[i];
i++;
}
while (!(SPI1->SR & SPI_SR_TXE)) {}; // wait for TXE bit to set -> This will indicate that the buffer is empty
while (SPI1->SR & SPI_SR_BSY) {}; // wait for BSY bit to Reset -> This will indicate that SPI is not busy in communication
// Clear the Overrun flag by reading DR and SR
__IO uint32_t temp = SPI1->DR;
temp = SPI1->SR;
}
char* myTxData = "Hello World!";
int main(void)
{
HAL_Init();
SystemClock_Config();
GPIOConfig();
SPIConfig();
SPI_Enable();
while (1)
{
HAL_Delay(1000);
CSN_Enable();
SPI_Transmit(myTxData, 11);
CSN_Disable();
}
}
Solved! Go to Solution.
2021-06-25 8:15 AM
SPI-> DR is sensible to write size. Try:
* ((__IO uint8_t *) & pSpi->DR) = (uint8_t) data [i] ;
2021-06-25 1:17 AM
It seems to be adding 0x00 after every character sent.
2021-06-25 8:15 AM
SPI-> DR is sensible to write size. Try:
* ((__IO uint8_t *) & pSpi->DR) = (uint8_t) data [i] ;