cancel
Showing results for 
Search instead for 
Did you mean: 

Recovery ST-Link bootloader

x893
Associate II
Posted on January 12, 2011 at 20:01

Hello

is any way to recovery ST-Link bootloader ?
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
Posted on January 12, 2011 at 22:52

Yes

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
atdyer
Associate
Posted on January 31, 2011 at 18:01

Hi Clive,

just joined the forum, I've got 2 STM32 Discovery boards and have used one to program the others STM32F103C8T6 to play with the keil USB mass memory demo, overwriting the embedded ST-LINK.

I know I can use the second STM32 to program either of the embedded STM32's on the second board, but would like to restore the original embedded firmware at the moment.

How can I recover the ST-LINK bootloader?

shakedyaniv
Associate II
Posted on August 18, 2011 at 13:13

shakedyaniv
Associate II
Posted on August 18, 2011 at 13:16

shakedyaniv
Associate II
Posted on August 18, 2011 at 13:17

shakedyaniv
Associate II
Posted on August 18, 2011 at 13:19

shakedyaniv
Associate II
Posted on August 18, 2011 at 13:20

x8932
Associate II
Posted on October 25, 2011 at 07:41

I not see any suggestions to recovery ST-Link. Can you repost this info (if possible)

Thanks in advance
Posted on November 01, 2011 at 20:53

I not see any suggestions to recovery ST-Link. Can you repost this info (if possible)

The original question was is it possible. There are several parts to the firmware, do you have the application portion? If you do, then you have control of the part, and can emit the 0x08000000..0x08003FFF portion in any number of ways.

If you have all the pieces you can push it back in via the BOOTx/USART1 method.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..