cancel
Showing results for 
Search instead for 
Did you mean: 

SPİ SCK frequency ?

A.Caliskan
Associate II

hello , I use spi and ı use slave mod spi. When I send a frequency of 500khz or more as a clock so data is shifting or I recieve wrong data but I send a frequency less than 500 khz I recieve true data. what is the reason of this.( use stm32h743zı)

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
KnarfB
Super User

Hook up a logic analyzer, even a cheap USB one or better a scope and check the timing/waveforms. Maybe the waveforms are bad and the timing works only for lower clocks. Or the sampling point (SPI mode) is wrong. Do you handle a SS/CS pin? Maybe that handling is too slow.

hth

KnarfB

I dont use cs/ss pin and ı check waveforms no problem appears,

> recieve wrong data

are bits flipped or shifted? Always the same pattern or random? Can you force specific bit patterns (0xFF, 0x55, 0xAA,...) for better testing?

for example I send 0xC1BA(1100 0001 1011 1010) and I check pin with oscilloscope I see 0x8375(1000 0011 1011 0101), data is 1 bit shift left but if frequency is less than 500 khz no problem.

TDK
Super User

Sounds like slave is not ready to receive when the master sends the first bit. And/or incorrect CPHA/CPOL settings.

>  ı check waveforms no problem appears,

Show them. The problem is somewhere and it's unlikely to be an STM32 hardware issue. Show relevant code.

If you feel a post has answered your question, please click "Accept as Solution".