[SOLVED] STM32F746G-DISCO -- SPI connection to PGA2311---
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-20 7:22 AM
I have the STM32F746G-DISCO and after some good result with I2C bus I would like to interface a PGA2311 with SPI.
This code hang the STM32 processor, why ?
#include "stm32f7xx_hal_spi.h"
SPI_HandleTypeDef spi = { .Instance = SPI2 };
void BSP_SPI_Init()
{
__GPIOB_CLK_ENABLE();
__GPIOI_CLK_ENABLE();
__SPI1_CLK_ENABLE();
spi.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
spi.Init.Direction = SPI_DIRECTION_2LINES;
spi.Init.CLKPhase = SPI_PHASE_1EDGE;
spi.Init.CLKPolarity = SPI_POLARITY_LOW;
spi.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;
spi.Init.DataSize = SPI_DATASIZE_8BIT;
spi.Init.FirstBit = SPI_FIRSTBIT_LSB;
spi.Init.NSS = SPI_NSS_HARD_OUTPUT;
spi.Init.TIMode = SPI_TIMODE_DISABLED;
spi.Init.Mode = SPI_MODE_MASTER;
if (HAL_SPI_Init(&spi) != HAL_OK)
{
__asm("bkpt 255");
}
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_14 | GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
//GPIO_InitStruct.Alternate = GPIO_AF5_SPI1; ??
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
//GPIO_InitStruct.Alternate = GPIO_AF5_SPI1; ??
HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);
// CS pin
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);
}
void BSP_SPI_Write(uint8_t Value)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);
HAL_SPI_Transmit(&spi, (uint8_t *)&Value, 1, HAL_MAX_DELAY);
HAL_SPI_Transmit(&spi, (uint8_t *)&Value, 1, HAL_MAX_DELAY);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);
}
- Labels:
-
SPI
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-20 7:52 AM
Solved the hang but still not work
SPI_HandleTypeDef spi = { .Instance = SPI2 };
void BSP_SPI_Init()
{
__GPIOB_CLK_ENABLE();
__GPIOI_CLK_ENABLE();
__SPI2_CLK_ENABLE(); <<<<<<< SPI2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-20 8:28 AM
Define "does not work". What are you seeing, or NOT seeing? And you still have the "alternate" assignment commented out in your GPIO init code, so the SPI port won't be connected to those pins. Instead the pins will be connected to whatever random value is in that structure member. I don't recall who keeps suggesting this, maybe @Community member​ or @Community member​, but for REPEATABLE code, unless you are explicitly assigning values to EVERY structure member, declare your structure variable like this:
GPIO_InitTypeDef GPIO_InitStruct = {0};
Then at least it will contain the same, known data every time you run the program, which makes it WAAAAAAY easier to debug things.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-20 8:55 AM
Solved all ok
SPI2_MOSI is SPI output
SPI2_SCK is SPi clock out
PA8 is the CS pin
void BSP_SPI_Init()
{
__GPIOB_CLK_ENABLE();
__GPIOI_CLK_ENABLE();
__SPI2_CLK_ENABLE();
spi.Instance = SPI2;
spi.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
spi.Init.Direction = SPI_DIRECTION_2LINES;
spi.Init.CLKPhase = SPI_PHASE_1EDGE;
spi.Init.CLKPolarity = SPI_POLARITY_LOW;
spi.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;
spi.Init.CRCPolynomial = 7;
spi.Init.DataSize = SPI_DATASIZE_8BIT;
//spi.Init.FirstBit = SPI_FIRSTBIT_LSB;
spi.Init.FirstBit = SPI_FIRSTBIT_MSB;
//spi.Init.NSS = SPI_NSS_HARD_OUTPUT;
spi.Init.NSS = SPI_NSS_SOFT;
spi.Init.TIMode = SPI_TIMODE_DISABLED;
spi.Init.Mode = SPI_MODE_MASTER;
if (HAL_SPI_Init(&spi) != HAL_OK)
{
__asm("bkpt 255");
}
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_PIN_14 | GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);
// CS pin
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);
}
void BSP_SPI_Write(uint8_t Value)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);
HAL_SPI_Transmit(&spi, (uint8_t *)&Value, 1, HAL_MAX_DELAY);
HAL_SPI_Transmit(&spi, (uint8_t *)&Value, 1, HAL_MAX_DELAY);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);
}