cancel
Showing results for 
Search instead for 
Did you mean: 

skip flash erase before programming

RobNeWin
Associate II

hello,

Which command is valid to do this? I see --skipErase, I have also seen --ske, or ske as possible commands to use.

What is the syntax for this command? I dont see a reference in the manual...

Please help thanks in advance.

2 REPLIES 2
Foued_KH
ST Employee

Hello @RobNeWin​ ,

The equivalent of 'Skip Flash Erase' option is 'ske' to be used with ST-LINK_CLI.exe.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

@KHALSI_Foued​  great, what is the syntax to send this command?

Do I do this before the download (-w)? or after? or a separate command?

thanks!