Solved
Simple UART problem STM32H753
Hi,
I'm relatively new to the STM32 world and I'm becoming frustrated that I can't make a simple UART work. No DMA, no interrupts just trying to send bytes out of the UART and then receive them. Here is my setup code:
void UART7_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
HAL_Init();
/* Peripheral clock enable */
__HAL_RCC_UART7_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
/**UART7 GPIO Configuration
PF6 ------> UART7_RX
PF7 ------> UART7_TX
PF8 ------> UART7_RTS
PF9 ------> UART7_CTS
*/
GPIO_InitStruct.Pin = U7_PAY_RX_SPI5_NSS_Pin|U7_PAY_TX_SPI5_SCK_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_UART7;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
huart7.Instance = UART7;
huart7.Init.BaudRate = 115200;
huart7.Init.WordLength = UART_WORDLENGTH_8B;
huart7.Init.StopBits = UART_STOPBITS_1;
huart7.Init.Parity = UART_PARITY_NONE;
huart7.Init.Mode = UART_MODE_TX_RX;
huart7.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart7.Init.OverSampling = UART_OVERSAMPLING_16;
huart7.Init.OneBitSampling = UART_ONEBIT_SAMPLING_DISABLED;
huart7.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if(HAL_UART_Init(&huart7) != HAL_OK)
{
asm("bkpt 255"); // Just for degugging
Error_Handler();
}
/* UART7 interrupt Init */
//HAL_NVIC_SetPriority(UART7_IRQn, 5, 0);
//HAL_NVIC_EnableIRQ(UART7_IRQn);
/* USER CODE BEGIN UART7_MspInit 1 */
/* USER CODE END UART7_MspInit 1 */
}
And here is the actual transmit code:
do
{
drv_led_toggle(DRV_LED_ID_AMBER);
HAL_UART_Transmit(&huart7, receiveBuffer, sizeof(receiveBuffer), TIMEOUT);
HAL_Delay(300);
//HAL_UART_Receive(&huart7, receiveBuffer, 1, TIMEOUT);
drv_led_toggle(DRV_LED_ID_AMBER);
HAL_Delay(300);
if(UART7->ISR & (1<<5))
{
HAL_UART_Receive(&huart7, receiveBuffer , 1 /*sizeof(receiveBuffer)*/, TIMEOUT);
}
if(i%2)drv_led_toggle(DRV_LED_ID_AMBER);
} while(i<5);
I'm pretty sure that it's something simple and I'm just missing it. Any advice is appreciated.
Thanks.