2013-10-14 3:47 AM
Hi,
I am trying to drive a servo motor(for this case, TowerPro MG90S), so I want to get 50 hz frequency and duty cycle between %5 and %10. My board is STM32F407 Discovery. I tried to change Peripheral Lib example a little bit. It says that APB1 frequency has prescaler other than 1, so it will be multiplied by 2. As I calculated, timer3 frequency has to be 84 Mhz in this case. Afterwards, I am setting prescaler value as 42-1=41 and ARR = 4000-1=3999. The result is, servo is not driven. When I change prescaler as 84-1=83, it is working. So, Is Timer3clk 168Mhz? How can it be possible? TIM_TimeBaseStructure.TIM_Period = 3999; TIM_TimeBaseStructure.TIM_Prescaler = 83; In the statuation that prescaler is 83 and ARR is 3999, the motor is driven. I assigned CCR values from 200 to 400. Here is another problem due to motor is turning about 90 degrees. When I changed it from about 150 to about 500, it is turning about 180 degrees. Firstly I am tried to arrange duty cycle between %5 and %10, secondly I found this numbers after a lot of attemptions. I couldn't understand how it is working, can you help me to understand these? Thanks for your time. #stm32 #timer #pwm #discovery #output2013-10-14 4:21 AM
So basic math issues here
With 42,4000 for a 84 MHz clock we have 84000000 / (42 * 4000) = 500 Hz? What you really probably want is 84000000/ (84 * 20000) = 50 Hz So a Prescaler of 84-1 to get your TIM clocking at 1 MHz (1 us ticks) and a Period of 20000-1 to get a TIM period at 50 Hz (20 ms ticks) The value then written to Pulse (CCRx) then relects the ON TIME in microseconds, presumably something between 600 us (3%) and 2400 us (12%)? Right?2013-10-14 4:42 AM
Hi,
Thanks for the correction, I changed my values with yours. I want to drive them using hardware pwm without interrupts, so I ported the codes in link: TIM_TimeBaseStructure.TIM_Period = 20000-1; TIM_TimeBaseStructure.TIM_Prescaler = 84-1; I assigned CCR values in the range of 1000 and 2000. But now the servo is not running. I found a code running with this values: TIM_TimeBaseStructure.TIM_Period=400; TIM_TimeBaseStructure.TIM_Prescaler=839; In this code, 84000000/840 gives 100000 and 100000/400 gives 250 Hz. I cant understand why servo is working with this.2013-10-14 5:01 AM
I cant understand why servo is working with this.
Yes, well then you'll need to put a scope on the pin and see what signal you're actually generating. It could be you are not clocking the STM32F4 at the speed you think you are. I don't have a spec sheet for the servo.2013-10-14 5:07 AM
Thanks, this week is holiday on my country, I dont have a scope or logic analyzer with me for now. In a couple of days I will check the output with a scope and write the results.
2013-10-14 5:32 AM
You could benchmark the clock using the RTC, or blinking an LED at 1 Hz.
Check also HSE_VALUE reflects the 8 MHz used by the STM32F4-Discovery boards, and the PLL/clock settings in system32_stm32f4xx.c2013-10-14 6:51 AM
Hi, I spend some time debugging and realized that the system uses HSI as clock source. So it explains why it is working at 16Mhz instead of 84 Mhz.
I called SystemCoreClockUpdate() function in the system_stm32f4xx.c file, afterwards see that tmp variable is set as ''0''. I dont know why it is not starting with external osilator and not using pll, so I will learn how to change it to use HSE at 168Mhz. Thank you for your time.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.