Sending one byte via SPI STM32G474
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 3:14 AM
I need to send data one byte at a time via SPI. After transferring the byte, I set "Chip Select" from the program to state 1. I track the end of the transfer by the BSY bit in the SPI_SR register. But the microcontroller transmits two bytes, the first byte is the value from the DR register and the second byte 0. The transmission length is set to 8 bits. I tried to set a different transmission length, but the microcontroller always sends two transmissions of the length I set. Below is the initialization code.
RCC-> APB2ENR | = RCC_APB2ENR_SPI4EN;
// CPHA = 1 // CPOL = 1
SPI4-> CR1 =
SPI_CR1_BR_1 | SPI_CR1_BR_2 | SPI_CR1_BR_0 | // Baud rate = Fpclk / 256
SPI_CR1_MSTR |
SPI_CR1_CPOL |
SPI_CR1_CPHA |
SPI_CR1_SSM |
SPI_CR1_SSI;
SPI4-> CR2 = SPI_CR2_DS_0 | SPI_CR2_DS_1 | SPI_CR2_DS_2;
SPI4-> CR1 | = SPI_CR1_SPE;
Send data
LCD_CS_Clr();
_delay_us(2);
SPI4->DR = data;
while((SPI4->SR & SPI_SR_BSY) != 0);
_delay_us(2);
LCD_CS_Set();
_delay_us(2);
Solved! Go to Solution.
- Labels:
-
SPI
-
STM32G4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 3:18 AM
The assignment SPI4->DR = data; is wider than 8-Bits so 2 bytes are sent.
Try
*(__IO uint8_t*)(&SPI4->DR) = data;
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 3:18 AM
The assignment SPI4->DR = data; is wider than 8-Bits so 2 bytes are sent.
Try
*(__IO uint8_t*)(&SPI4->DR) = data;
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 3:27 AM
Thanks KnarfB, it really works.
I am using data of type uint8_t. How does DR register type conversion affect transfer?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 3:51 AM
Probably the SPI IP evaluates the byte lanes from the access protocoll..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 4:02 AM
The definition of SPI DR in CMSIS is
__IO uint32_t DR;
which makes it a 32-bit type variable (8 bit would not be enough for all possible SPI data sizes, up to 16 bit are possible).
Therefore, data is promoted to an unsigned int in the assignment and data is stored using a 32-bit STR instruction.
But, the SPI DR register HW is implemented that it switches to 8-bit only if 8-bit are written (STRB instruction).
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 4:57 AM
Thanks, it helped me a lot.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-29 4:59 AM
I solved the problem. KnarfB's suggestion helped.