2021-05-31 12:46 AM
i'm trying to communicate with a Wifi module (esp8266) using STM32F103, on keil IDE. As described in the schematic : i want making my stm32 send AT command to esp8266 through usart1 (Tx1), and getting the esp response (Rx1), then display the esp response on computer serial monitor using usart2 ( Tx2).
After configuring usart1 and usart2, and writing the functions to send an receive data, i'm getting only the ECHO of the command, rather than the response which should be "OK"
. when i'm sending "AT\r\n", i'm receiving only AT on serial monitor. i will share the code i have wrote, and the traces on logic analyzer. if there is any suggestion i will be thankful.
int len=0;
char buff[256];
int main(void){
__disable_irq();
systick_init();
UART1_Init();
UART2_Init();
Delayms(100);
printMsg1("AT\r\n");
Delayms(100);
NVIC_EnableIRQ(USART1_IRQn);
__enable_irq();
while(1){}
}
void USART1_IRQHandler(){
if (USART1->SR & USART_SR_RXNE) // if received data (RXNE event flag is set) is ready to be read -->RXNE
{
buff[len] = USART1->DR;
Delayms(100);
printMsg2(buff);
}
}
void printMsg1(char *msg, ...) // Sending AT command to ESP ( Stm32-> ESP8266)
{
va_list args;
va_start(args,msg);
vsprintf(buff,msg,args);
for(int i=0;i<strlen(buff);i++)
{
USART1->DR = (buff[i]&0xFF);
while(!(USART1->SR & USART_SR_TXE)); //wait for TXE, 1 = data transferred
}
}
void printMsg2(char *msg, ...) // Sending ESP response to Serial Monitor ( STM32-> PC)
{
va_list args;
va_start(args,msg);
vsprintf(buff,msg,args);
for(int i=0;i<strlen(buff);i++)
{
USART2->DR = buff[i];
while(!(USART2->SR & USART_SR_TXE)); //wait for TXE, 1 = data transferred
}
}
Solved! Go to Solution.
2021-06-01 3:35 AM
This is the code modifed : it works fine :
#include "stm32f10x.h" // Device header
#include <stdio.h>
#include "stdint.h"
#include "stdarg.h"
#include "string.h"
#include "Msg_Handle.h"
#include <string.h>
void UART2_Init(void);
void UART1_Init(void);
void USART1_IRQHandler(void);
void DelayTimerUs(int n);
//UART1 --> MCU to Wifi
//UART2 --> MCU to Serial monitor
void UART2_Init(){
//1) Enable USART2 clock and Porta clock (PA2-->Tx & PA3-->Rx)
RCC->APB1ENR |= RCC_APB1ENR_USART2EN;
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN;
//2) Configuring Tx2 to be used as Alternate function (Special I/O) push-pull output
GPIOA->CRL &=~ GPIO_CRL_CNF2_0;
GPIOA->CRL |= GPIO_CRL_CNF2_1;
GPIOA->CRL |= (GPIO_CRL_MODE2_1 | GPIO_CRL_MODE2_0);
//3) Configuring Rx3 to be used as Alternate function (Special I/O) Float input
GPIOA->CRL &=~ GPIO_CRL_MODE3_0 | GPIO_CRL_MODE3_1; // 10MHz Rx PA3
GPIOA->CRL &=~ GPIO_CRL_CNF3_1 ;
GPIOA->CRL |= GPIO_CRL_CNF3_0;
//3) Set the Baud rate
// USART2->BRR = 0XEA6; // 9600
USART2->BRR = 0X138; // 115200
//4) CR1 register (Enable usart)
USART2->CR1 |= USART_CR1_TE;
USART2->CR1 |= USART_CR1_RE ;
USART2->CR1 |= USART_CR1_UE;
}
void UART1_Init(){
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN | RCC_APB2ENR_AFIOEN | RCC_APB2ENR_USART1EN; //clock to GPIO A enabled, alt.funct.en, USART1 clock enabled
GPIOA->CRH |= GPIO_CRH_CNF9_1 | GPIO_CRH_MODE9_0 | GPIO_CRH_MODE9_1; //port A9
GPIOA->CRH &= ~GPIO_CRH_CNF9_0; //port A9 is TX pin
GPIOA->CRH &= ~(GPIO_CRH_MODE10_0|GPIO_CRH_MODE10_1); //port A10 is RX pin
GPIOA->CRH |= GPIO_CRH_CNF10_0; //port A10 is RX pin*/
USART1->BRR = 0X271; // 115200
USART1->CR1 |= USART_CR1_TE;
USART1->CR1 |= USART_CR1_RE ;
USART1->CR1 |= USART_CR1_UE;
USART1->CR1 |= USART_CR1_RXNEIE | USART_CR1_TXEIE ;
}
void USART1_IRQHandler(){
if (USART1->SR & USART_SR_RXNE) // if received data (RXNE event flag is set) is ready to be read -->RXNE
{
buff_read[len] = USART1->DR;
printMsg2(buff_read);
}
}
int len=0;
char buff[256];
char buff_read[256];
void DelayTimerUs(int n){
// 1 Mhz ---> 1Us
//ARR = n (n=1 --> 1us) (n=2 --> 2us) ....
RCC->APB1ENR |= RCC_APB1ENR_TIM2EN;
TIM2->PSC = 36;
TIM2->ARR = n;
TIM2->CNT = 0;
TIM2->CR1 = TIM_CR1_CEN;
for( int i =0; i<n; i++){
while (!(TIM2->SR & (1<<0))) {}
}
TIM2->SR &=~ (1<<0);
TIM2->CR1 &=~ TIM_CR1_CEN;
}
int main(void){
__disable_irq();
systick_init();
UART1_Init();
UART2_Init();
printMsg1("AT\r\n");
DelayTimerUs(1000);
printMsg1("AT+RESTORE\r\n");
DelayTimerUs(1000);
printMsg1("AT+CWMODE=1\r\n");
DelayTimerUs(1000);
NVIC_EnableIRQ(USART1_IRQn);
__enable_irq();
while(1){}
}
2021-05-31 6:57 AM
I don't see "AT\r\n\" or "OK" in your logic analyzer plot. I do see that it indicates frame errors on the RX line. Doesn't seem like your baud rate matches what the logic analyzer is set to expect.
Probably not a problem here, but generally you should reverse the order here so it waits for TXE before sending a byte instead of blocking until the transmission is finished.
USART2->DR = buff[i];
while(!(USART2->SR & USART_SR_TXE)); //wait for TXE, 1 = data transferredYou're also sending "AT\r\n" without interrupts enabled, so any response is going to get ignored, unless it's sent 100+ms after the message ends.
__disable_irq();
...
printMsg1("AT\r\n");
Delayms(100);
NVIC_EnableIRQ(USART1_IRQn);
__enable_irq();
2021-05-31 9:24 AM
deleted
2021-05-31 9:24 AM
Thank's for reply,
The baud rate is set at 115200 for stm32, esp8266 and logic analyzer.
I've tried these suggestions, when enabling interrupt then sending "AT\r\n", i get nothing on serial monitor, Rx, Tx are held high (logic analyzer)
2021-05-31 10:55 AM
You're saying the values match, but your plot suggests otherwise. Possible your HSE_VALUE is incorrect. Put out a known frequency signal such as MCO on a pin and verify the clock is what you think it is.
2021-05-31 12:42 PM
TXE indicates the buffer is empty, and can take data, you should be FRONT CHECKING it, not back checking
I don't understand the delay in the interrupt, or the non-incrementing buffer pointer, and the use of string, lack of NUL termination, and then reuse of the same buffer in printMsg2
Why can't you do a simple echo of each byte received from USART1 in the IRQ handler to USART2?
2021-06-01 3:32 AM
it turns out that the "Delayms" function corrupted or caused the losses of the received data , perhaps this is due to the fact that the long waiting time leads to the loss of data.
Furthemore:
the same buffer is used for sending the AT command and receiving the response "buff[len]",
which place the receiving data also in buff[len] and seems to be ignored,
this is why i'm receiving the command echo.
2021-06-01 3:32 AM
it turns out that the "Delayms" function corrupted or caused the losses of the received data , perhaps this is due to the fact that the long waiting time leads to the loss of data.
Furthemore:
the same buffer is used for sending the AT command and receiving the response "buff[len]",
which place the receiving data also in buff[len] and seems to be ignored,
this is why i'm receiving the command echo.
2021-06-01 3:35 AM
This is the code modifed : it works fine :
#include "stm32f10x.h" // Device header
#include <stdio.h>
#include "stdint.h"
#include "stdarg.h"
#include "string.h"
#include "Msg_Handle.h"
#include <string.h>
void UART2_Init(void);
void UART1_Init(void);
void USART1_IRQHandler(void);
void DelayTimerUs(int n);
//UART1 --> MCU to Wifi
//UART2 --> MCU to Serial monitor
void UART2_Init(){
//1) Enable USART2 clock and Porta clock (PA2-->Tx & PA3-->Rx)
RCC->APB1ENR |= RCC_APB1ENR_USART2EN;
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN;
//2) Configuring Tx2 to be used as Alternate function (Special I/O) push-pull output
GPIOA->CRL &=~ GPIO_CRL_CNF2_0;
GPIOA->CRL |= GPIO_CRL_CNF2_1;
GPIOA->CRL |= (GPIO_CRL_MODE2_1 | GPIO_CRL_MODE2_0);
//3) Configuring Rx3 to be used as Alternate function (Special I/O) Float input
GPIOA->CRL &=~ GPIO_CRL_MODE3_0 | GPIO_CRL_MODE3_1; // 10MHz Rx PA3
GPIOA->CRL &=~ GPIO_CRL_CNF3_1 ;
GPIOA->CRL |= GPIO_CRL_CNF3_0;
//3) Set the Baud rate
// USART2->BRR = 0XEA6; // 9600
USART2->BRR = 0X138; // 115200
//4) CR1 register (Enable usart)
USART2->CR1 |= USART_CR1_TE;
USART2->CR1 |= USART_CR1_RE ;
USART2->CR1 |= USART_CR1_UE;
}
void UART1_Init(){
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN | RCC_APB2ENR_AFIOEN | RCC_APB2ENR_USART1EN; //clock to GPIO A enabled, alt.funct.en, USART1 clock enabled
GPIOA->CRH |= GPIO_CRH_CNF9_1 | GPIO_CRH_MODE9_0 | GPIO_CRH_MODE9_1; //port A9
GPIOA->CRH &= ~GPIO_CRH_CNF9_0; //port A9 is TX pin
GPIOA->CRH &= ~(GPIO_CRH_MODE10_0|GPIO_CRH_MODE10_1); //port A10 is RX pin
GPIOA->CRH |= GPIO_CRH_CNF10_0; //port A10 is RX pin*/
USART1->BRR = 0X271; // 115200
USART1->CR1 |= USART_CR1_TE;
USART1->CR1 |= USART_CR1_RE ;
USART1->CR1 |= USART_CR1_UE;
USART1->CR1 |= USART_CR1_RXNEIE | USART_CR1_TXEIE ;
}
void USART1_IRQHandler(){
if (USART1->SR & USART_SR_RXNE) // if received data (RXNE event flag is set) is ready to be read -->RXNE
{
buff_read[len] = USART1->DR;
printMsg2(buff_read);
}
}
int len=0;
char buff[256];
char buff_read[256];
void DelayTimerUs(int n){
// 1 Mhz ---> 1Us
//ARR = n (n=1 --> 1us) (n=2 --> 2us) ....
RCC->APB1ENR |= RCC_APB1ENR_TIM2EN;
TIM2->PSC = 36;
TIM2->ARR = n;
TIM2->CNT = 0;
TIM2->CR1 = TIM_CR1_CEN;
for( int i =0; i<n; i++){
while (!(TIM2->SR & (1<<0))) {}
}
TIM2->SR &=~ (1<<0);
TIM2->CR1 &=~ TIM_CR1_CEN;
}
int main(void){
__disable_irq();
systick_init();
UART1_Init();
UART2_Init();
printMsg1("AT\r\n");
DelayTimerUs(1000);
printMsg1("AT+RESTORE\r\n");
DelayTimerUs(1000);
printMsg1("AT+CWMODE=1\r\n");
DelayTimerUs(1000);
NVIC_EnableIRQ(USART1_IRQn);
__enable_irq();
while(1){}
}
2021-06-08 7:10 AM
Hello @SIDRI.1,
Please mark the helped reply as Best answer (click on "Select as Best"), to help others get the answer quickly.
Mohamed Aymen.