2012-04-20 10:42 PM
seection of accelrerometer IC for car crash detection. which parameter need to consider,
please suggest which IC is best. Which g level is required. please let me know thank you2012-04-21 05:14 AM
You need to find someone qualified to answer/develop the solution. Random people on the internet should not be relied upon for life critical design parameters.
You need to know the initial speed/velocity, and the time/distance required to come to rest. You might be able to get some number from local insurance/government labs about the forces in crashes from vehicle crash testing. The results from USA might not be applicable to vehicles in other markets with more lax safety requirements. The G forces of hitting a concrete wall at speed are going to be very high, it's going to stop very quickly and the distance travelled will be the deformation of the vehicle. Hitting a pedestrian at similar speeds will have significantly less impact. Many accidents are considered insufficient to deploy an air bag, and depend on the direction of the impact.http://www.hwycom.com/safetyCrashTest60.php