cancel
Showing results for 
Search instead for 
Did you mean: 

Dual UARTs Problem

nickabrham
Associate II
Posted on April 21, 2012 at 08:27

Hi Everyone,

I have developed a program on STM3210E-Eval, in which I have configured both USART1 and USART2 to send data on their respective interrupts. Unfortunately only USART2 is sending data. UART1 is not sending the data. Attached file contains the relevant files. Kindly help.

Bye,

Nick.

 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on April 21, 2012 at 14:28

You want to initialize USART1, not USART2

ie USART_Init( USART2, &USART_InitStructure); // Configure the USART1 should be USART_Init( USART1, &USART_InitStructure); // Configure the USART1

// Configure UART1
void UART1_Configuration(void)
{
// USART1 configured as follow:
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure); // Configure the USART1
//Enable the USART Transmit interrupt: this interrupt is generated when the
//USART1 transmit data register is empty
USART_ITConfig(USART1, USART_IT_TXE, ENABLE);
//Enable the USART Receive interrupt: this interrupt is generated when the
//USART1 receive data register is not empty
USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);
//Enable USART1
USART_Cmd(USART1, ENABLE);
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
nickabrham
Associate II
Posted on April 21, 2012 at 15:16

Thanks Clive,