cancel
Showing results for 
Search instead for 
Did you mean: 

SDIO works well in SD-1bit mode but not in SD 4bit mode

Yang Yang
Associate III

I am using cubemx generated SD card test code on a custom board. And everything looks fine in SD 1bit mode, I can create new file, read and write data to it correctly. But when I am using 4bit mode, the f_open() function stalls. What might be the problem?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee

Hello @Yang Yang​ ,

Which device are you using ?

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Might not be wired properly, ie mixed bits, too long, no pull-ups, etc.

4-bit mode sensitive to relative bit skewing

Not much to work with, engineering shouldn't need to be a guessing game. Present a more complete context for your problem.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi, Clive

STM32F415RGT6 MCU is used. And I am quite sure the connections between MCU and microSD card is correct. So I think we can focus on the software side.

Best Regards

Yang