2014-07-06 2:48 AM
Hi, guys,
please reassure me if I missed something. I wanted to use SDIO and TFT LCD driver module at the same time on a 144-pin STM32F429 of my own design..but it seems I can't Both SDIO_D2 and LCD_R2 signals can only be mapped to PC10 pin. SD card could be used in 1bit mode..but I want 4bit access for speed, so I need SDIO_2. Any idea on a workaround? regards, Tommy #port-mapping-stm32f429-sdio-tft2014-07-06 4:07 AM
It's not you, ST made some frustratingly poor choices with their pin muxing strategy. You really need to consider higher pin count devices to get all the interfaces out.
2014-07-06 7:17 AM
Thanks, Clive...it was hard to believe.
Especially because SD card reading + TFT driving can be considered twin functions. And there is only a single problem pin : SDIO_D0,_D1,_D3,_CK,_CMD are okay, SDIO_D2 and LCD_R2 are both un-remappably fixed to PC10. On 176 pincount devices LCD_R2 may be mapped to PH8..I'm gonna use that instead. cheers, Tommy