2008-08-18 8:10 AM
SD card interface problem
2011-05-17 3:42 AM
Hi, I've a strange problem with some code I've ported to my stm32 board.
I need to interface with a SD card through the SPI port. The code works reasonably well if I test it under emulation (I'm using openocd and a JTAG USB OCD Programmer), I can retrieve the card identification register, the card specific data register and read block of data. If I detach the board from the jtag programmer and reset, then the program fails to identify the SD card. Before continuing I'd like to solve this issue, anyone have an idea what could be the problem?