2015-03-23 5:06 PM
I'm Using Keil on an STM32F439 on a little project.
I am trying something that does this:Set framebuffer to the location of an image whose width is 3 times that of the screenset line pitch to 3*X_RESOLUTION display image.Will the stm32 do this correctly?Right now I am getting a strange mix of all 3 columns of the image2015-03-24 2:10 PM
an update:
It seems what is happning is regardless of what I set the line pitch to, it is taking it as 320*2 (2 bytes per pixel and the horizontal resolution)