2015-11-17 6:09 AM
Hello,
It seems that the IRQ handler for the wakeup does not trigger even the RTC is running correctly, WUTIE is set in CR register and the ISR flag WUTF is set as expected. What could be the issue? The FW is build with GCC. What could be the issue? Thanks in advance.Here is the code:void v_Rtc_Initialise(void)
{ EXTI_InitTypeDef t_wut_interrupt; // Allow access to RTC RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); PWR_RTCAccessCmd(ENABLE); RTC_WriteProtectionCmd(DISABLE); // Enable the LSE OSC RCC_LSEConfig(RCC_LSE_ON); // Wait for LSE to settle. while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) { __NOP(); } /* Select the RTC Clock Source */ RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); // Disable all interrupt sources and clear flags. RTC_ITConfig(RTC_IT_TS | RTC_IT_WUT | RTC_IT_ALRA | RTC_IT_ALRB | RTC_IT_TAMP, DISABLE); RTC_ClearFlag(RTC_FLAG_TAMP1F | RTC_FLAG_TSOVF | RTC_FLAG_TSF | RTC_FLAG_WUTF | RTC_FLAG_ALRBF | RTC_FLAG_ALRAF | RTC_FLAG_RSF); /* EXTI configuration */ EXTI_ClearITPendingBit(EXTI_Line20); t_wut_interrupt.EXTI_Line = EXTI_Line20; t_wut_interrupt.EXTI_Mode = EXTI_Mode_Interrupt; t_wut_interrupt.EXTI_Trigger = EXTI_Trigger_Rising; t_wut_interrupt.EXTI_LineCmd = ENABLE; EXTI_Init(&t_wut_interrupt); /* Enable the RTC Clock */ RCC_RTCCLKCmd(ENABLE); /* Wait for RTC APB registers synchronisation */ if (RTC_WaitForSynchro() == ERROR) { DEBUG_PRINT(1, ''RTC: Synchronisation failed.''); } /* RTC time base = LSE / ((AsynchPrediv+1) * (SynchPrediv+1)) = 1 Hz */ t_rtc_init.RTC_AsynchPrediv = 127; t_rtc_init.RTC_SynchPrediv = 255; t_rtc_init.RTC_HourFormat = RTC_HourFormat_24; if (RTC_Init(&t_rtc_init) == ERROR) { DEBUG_PRINT(1, ''RTC: Initialisation failed.''); } /* Set the Time */ t_rtc_time.RTC_Hours = 0x08; t_rtc_time.RTC_Minutes = 0x00; t_rtc_time.RTC_Seconds = 0x00; RTC_SetTime(RTC_Format_BCD, &t_rtc_time); /* Set the Date */ t_rtc_date.RTC_Month = RTC_Month_November; t_rtc_date.RTC_WeekDay = RTC_Weekday_Sunday; t_rtc_date.RTC_Date = 0x01; t_rtc_date.RTC_Year = 0x15; RTC_SetDate(RTC_Format_BCD, &t_rtc_date); if (RTC_WakeUpCmd(DISABLE) == ERROR) { DEBUG_PRINT(1, ''RTC: Wake up disable failed.''); } RTC_ClearFlag(RTC_FLAG_WUTF); RTC_WakeUpClockConfig(RTC_WakeUpClock_CK_SPRE_16bits);//(RTC_WakeUpClock_RTCCLK_Div4); PWR_RTCAccessCmd(DISABLE); return;}void v_Rtc_Set_Wakeup(uint32_t u32_wakeup_in_minutes){ PWR_RTCAccessCmd(ENABLE); RTC_WakeUpCmd(DISABLE); RTC_ITConfig(RTC_IT_WUT, DISABLE); DEBUG_PRINT(1, ''Debug: %u'', gu8_rtc_wut_debug); gu8_rtc_wut_debug = 0; if (u32_wakeup_in_minutes > 0) { if (u32_wakeup_in_minutes > WAKEUP_LIMIT) { DEBUG_PRINT(1, ''RTC: Wake up time too long, forced to 4369 minutes.''); u32_wakeup_in_minutes = WAKEUP_LIMIT; } //u32_wakeup_in_minutes *= 15; RTC_SetWakeUpCounter(u32_wakeup_in_minutes); RTC_ITConfig(RTC_IT_WUT, ENABLE); if (RTC_WakeUpCmd(ENABLE) == ERROR) { DEBUG_PRINT(1, ''RTC: Wake up enable failed.''); } } PWR_RTCAccessCmd(DISABLE); return;}void RTC_WKUP_IRQHandler(void){ gu8_rtc_wut_debug = 1; PWR_RTCAccessCmd(ENABLE); RTC_ClearFlag(RTC_FLAG_WUTF); EXTI_ClearITPendingBit(EXTI_Line20); RTC_ClearITPendingBit(RTC_IT_WUT); PWR_RTCAccessCmd(DISABLE); return;} #irqhandler #wakeup #rtc2015-11-18 12:32 AM
I made a test FW where I start a five second WUT and then print out the current register states to the serial. Here is short log:
DBG:Start WUT...
DBG:Time Count RTC-CR RTC-ISR IMR SWIER EXTIPR IRQDBG:08:00:00 5 4404 0033 102000 000000 000000 0DBG:08:00:01 5 4404 0033 102000 000000 000000 0DBG:08:00:02 5 4404 0033 102000 000000 000000 0DBG:08:00:03 5 4404 0033 102000 000000 000000 0DBG:08:00:04 5 4404 0033 102000 000000 000000 0DBG:08:00:05 5 4404 0033 102000 000000 000000 0DBG:08:00:06 5 4404 0433 102000 000000 100000 0DBG:08:00:07 5 4404 0433 102000 000000 100000 0DBG:08:00:08 5 4404 0433 102000 000000 100000 0DBG:08:00:09 5 4404 0433 102000 000000 100000 0DBG:08:00:10 5 4404 0433 102000 000000 100000 0DBG:08:00:11 5 4404 0433 102000 000000 100000 0DBG:08:00:12 5 4404 0433 102000 000000 100000 0DBG:08:00:13 5 4404 0433 102000 000000 100000 0DBG:08:00:14 5 4404 0433 102000 000000 100000 0The logs show that the WUTF is set correctly after five seconds and the EXTI20 is set as pending, but no IRQHandler call (IRQ on the log). This is frustrating.2015-11-18 1:05 AM
Problem solved! The code was missing configuration for NVIC vector. Now it works.