cancel
Showing results for 
Search instead for 
Did you mean: 

RTC in STM32L152RET6

chaitanya jasti
Associate II
Posted on February 28, 2017 at 07:52

h

i WE ARE USING

STM32L152RET6.Is it have internal RTC?

Why 

RTC_REFIN

RTC_TA RTC_OUT    pins are used?

Kindly provide any rtc document for STM32L152RET6

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Max
ST Employee
Posted on February 28, 2017 at 08:20

RTC_REFIN is used to synchronize with an external reference clock

RTC_TA is a tamper input

RTC_OUT is an alarm output 

you should definitely read the RTC section of 

https://www.google.com.sg/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&uact=8&ved=0ahUKEwiU8IiToLLSAhXFWiwKHfBjBgYQFggbMAA&url=http%3A%2F%2Fwww.st.com%2Fresource%2Fen%2Freference_manual%2Fcd00240193.pdf&usg=AFQjCNGgsDUGzTzCu9xmLvWPWWQzhSjtow

if you plan to use this device.

BR,

Max

Posted on February 28, 2017 at 11:58

IS THERE ANY HARDWARE CIRCUIT

On Tue, Feb 28, 2017 at 12:51 PM, Max <st-microelectronics@jiveon.com>

Posted on February 28, 2017 at 19:26

Review the EVAL and DISCOVERY series boards for the L1 series chips if you need to see viable schematics.

The device has an internal low speed oscillator (LSI), and can use a more precise external crystal (LSE) via the OSC_IN and OSC_OUT pins. There is an application note describing crystal/component selection.

Please learn to read and type in a coherent/professional manner, it will make communicating a lot easier.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 01, 2017 at 12:19

Hi,

Besides to Clive & Max proposals, I suggest you refer to

http://www.st.com/content/ccc/resource/technical/document/application_note/bf/94/f5/49/96/52/4e/75/CD00273528.pdf/files/CD00273528.pdf/jcr:content/translations/en.CD00273528.pdf

.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.