cancel
Showing results for 
Search instead for 
Did you mean: 

RM0316 Reference Manual STM32F303xx error

FordFairlane
Associate III
Posted on July 22, 2013 at 09:34

RM0316

15  Operational amplifier (OPAMP)

Table 54. Connections with dedicated I/O

OPAMP1 inverting input: PA3 (VM0)

PC5 (VM1)

15.4 OPAMP registers

15.4.1 OPAMP1 control register (OPAMP1_CSR)

Bit 8 VMS_SEL:

0: PC5 (VM0) used as OPAMP1 inverting input

1: PA3 (VM1) used as OPAMP1 inverting input

OPAMP2, OPAMP3 and OPAMP4 have the same errors.
1 REPLY 1
Amel NASRI
ST Employee
Posted on July 23, 2013 at 11:02

Hello,

Thanks for this feedback.

I checked the issue you reported & confirm it for OPAMP1, OPAMP2 and OPAMP3. For OPAMP4 there is no issue.

The correct information is in the registers description.

So, the table 54 needs to be fixed. This will be done in next reference manual release.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.