2025-11-28 6:36 AM - last edited on 2025-11-28 8:20 AM by mƎALLEm
Hello,
I expect this to be flagged before but couldnt find during search.
Is Table 116 for the stm32f43xx on page 768 missing registers for CRYP_K2LR / CRYP_K2RR at offset 0x30?
TIA
Solved! Go to Solution.
2025-12-03 6:26 AM
Hello @######
This is a feedback from our internal team:
The CRYP_K2LR and CRYP_K2RR registers are indeed present in the CRYP register map for the STM32F43xxx series. They are located at offsets 0x30 and 0x34 respectively, between the CRYP_K0RR (0x24) and CRYP_K3LR (0x38) registers.
In the provided section of Table 116, the intermediate lines between 0x24 and 0x38 are represented by “...”, which means that some registers, including CRYP_K2LR, CRYP_K2RR, as well as CRYP_K1LR and CRYP_K1RR, are included but not explicitly shown in this excerpt.
Therefore, these registers are well documented and are an integral part of the CRYP key registers. Moreover, this description is consistent with other reference manuals such as RM0455 for the STM32H7 series.
2025-11-28 6:39 AM - edited 2025-11-28 6:46 AM
Hello @###### and thank you for your contribution.
I will raise it internally and I will get back to you for any feedback. Internal ticket number for follow-up: 222783.
Thank you
2025-12-03 6:26 AM
Hello @######
This is a feedback from our internal team:
The CRYP_K2LR and CRYP_K2RR registers are indeed present in the CRYP register map for the STM32F43xxx series. They are located at offsets 0x30 and 0x34 respectively, between the CRYP_K0RR (0x24) and CRYP_K3LR (0x38) registers.
In the provided section of Table 116, the intermediate lines between 0x24 and 0x38 are represented by “...”, which means that some registers, including CRYP_K2LR, CRYP_K2RR, as well as CRYP_K1LR and CRYP_K1RR, are included but not explicitly shown in this excerpt.
Therefore, these registers are well documented and are an integral part of the CRYP key registers. Moreover, this description is consistent with other reference manuals such as RM0455 for the STM32H7 series.