2014-10-06 04:27 PM
Hi.
I am using the ST programmer to connect to my STM using SWD. I properly connected the GRD, SWDIO, SWCLK, and NRST. I can get some info from the STM as the version, revision... But i receive an error ''Can not connect to the device''.The revision is ''Y''. Is this revision not supported? How do I have to connect it to debug it properly??Thank you #error #support #stm322014-10-06 05:01 PM
What's running on the device?
Does it connect better if you choose the ''Connect under reset'' option? Most current ST-LINK firmwarehttp://developer.mbed.org/teams/ST/wiki/Nucleo-Firmware