2015-07-06 10:13 AM
I'm trying to decide if I want to use the STM32CUBE HAL code. Because I'm on linux, the cubemx thing doesn't run well, so I used the windows version and generated some code to use with openstm32 ( which also doesn't run well with linux ). I ignored all the openstm32 stuff and just created a new C project in standard eclipse. I setup all the include paths and symbols by hand.
I was feeling happy that I got it going without too much trouble and then I noticed this header in the linker script:/*
********************************************************************************* File : LinkerScript.ld**** Abstract : Linker script for STM32F103C8Tx Device with** 64KByte FLASH, 20KByte RAM**** Set heap size, stack size and stack location according** to application requirements.**** Set memory bank area and size if external memory is used.**** Target : STMicroelectronics STM32****** Distribution: The file is distributed as is, without any warranty** of any kind.**** (c)Copyright Ac6.** You may use this file as-is or modify it according to the needs of your** project. Distribution of this file (unmodified or modified) is not** permitted. Ac6 permit registered System Workbench for MCU users the** rights to distribute the assembled, compiled & linked contents of this** file as part of an application binary file, provided that it is built** using the System Workbench for MCU toolchain.*******************************************************************************Questions I have:1.) Is this intentional or just an overly cautious template in the cubemx code generator?2.) Are their other legal landmines lurking in the generated code that I should be aware of if my intent is to use this with open source code projects?-rick2015-08-11 2:28 AM
Hi Rickta59,
This issue is fixed with current SW4STM32 version available in AC6 site.Code generated by CubeMX as well as the examples available in the STM32CubeXX packages will not contain such restriction sentence in coming versions.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-07-06 5:27 AM
It's mid 2018 and this still the case with CubeMx 4.26.0.
2018-07-06 5:39 AM
'
It's mid 2018 and this still the case with CubeMx 4.26.0.'
that's the feature of consistency you get from Cube. free of charge, btw.