RESOLVED: Changing TIM PWM pulse width on the fly
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-13 4:13 PM
Posted on October 14, 2016 at 01:13
Hello,
I am using STM32F4 Discovery board (with STM32F407VGTx) with the latest HAL libraries. I am interested in varying PWM pulse width (duty ratio) in a while loop. Looking at MX_TIM3_Init function (also attached below), I see that sConfigOC.Pulse can be varied to change the pulse width. Can I simply do the following to vary the pulse width:while(1){
HAL_Delay(1000);
sConfigOC.Pulse = 100;
HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2);
HAL_Delay(1000);
sConfigOC.Pulse = 400;
HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2);
}//Here is the MX_TIM3_Init section:static void MX_TIM3_Init(void){ TIM_ClockConfigTypeDef sClockSourceConfig; TIM_MasterConfigTypeDef sMasterConfig; TIM_OC_InitTypeDef sConfigOC; htim3.Instance = TIM3; htim3.Init.Prescaler = 83; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 1350; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; if (HAL_TIM_Base_Init(&htim3) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_Init(&htim3) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 100; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_ENABLE; if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) != HAL_OK) { Error_Handler(); } HAL_TIM_MspPostInit(&htim3);}
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-10-14 3:19 AM
Posted on October 14, 2016 at 12:19
Hi Sel,
Try to do the update into interrput and not in the while loop.You can change these on the fly :
/* update the pulse value*/
TIM3->CCR1 = (Period * dutyCycle);
The new values will not take effect until the next update event (UEV).
To avoid a writing delay to the CCR1 register which can be the origin of a glitch, you should ensure that you have enabled the output compare preload OC1PE. In that way,Read/Write operations access the preloadregister, and TIMx_CCR1 preload value is loaded in the active register at each update event (UEV).
/* Enable the output compare 1 Preload */
TIM1->CCMR1 |= TIM_CCMR1_OC1PE;
-Hannibal-
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-18 11:30 PM
This worked fine for me! Thanks!