2023-11-11 8:39 AM
In my design, it is very important that a run-away MCU be stopped before it can do damage. In my case damage would occur if a specific MCU pin goes high for more than about 5 microseconds.
Are there any recommendations on the best way to do this (e.g., watchdog timer, Hard Fault interrupt)?
Solved! Go to Solution.
2023-11-11 9:29 AM - edited 2023-11-11 9:34 AM
so about hrtim -> protection of mosfet/driver
read in rm about hrtim -> fault protection !
the timer has break inputs, to stop output (go to save level - you have to define, what it should do.)
so "usual" way ( i use also) is: to have current limit protection , you need to test/measure the output current anyway;
you have as shown in circuit some current transformer - right? so use its signal to switch the break input; so you get over current protection (switching in ..some ns time outputs off ) and also protection against program errors.
just - test it working and never (also at power up or reset of cpu) any wrong signal is coming from the cpu pins - check with a DSO ! and only if 100% sure, its working fine AND protection also working, connect power to the mosfet part !!!! ( or you will blow up some xx mosfets for sure. :) )
2023-11-11 8:57 AM
is this again about the hrtim -> mosfet driving ?
2023-11-11 9:02 AM
Yes it is, but I thought my previous post was too complex to expect to get an answer. The answer to this post, would allow me to fix this issue as best as I can (about 1000 of these controllers are about to be built and I need them to work reliably).
2023-11-11 9:29 AM - edited 2023-11-11 9:34 AM
so about hrtim -> protection of mosfet/driver
read in rm about hrtim -> fault protection !
the timer has break inputs, to stop output (go to save level - you have to define, what it should do.)
so "usual" way ( i use also) is: to have current limit protection , you need to test/measure the output current anyway;
you have as shown in circuit some current transformer - right? so use its signal to switch the break input; so you get over current protection (switching in ..some ns time outputs off ) and also protection against program errors.
just - test it working and never (also at power up or reset of cpu) any wrong signal is coming from the cpu pins - check with a DSO ! and only if 100% sure, its working fine AND protection also working, connect power to the mosfet part !!!! ( or you will blow up some xx mosfets for sure. :) )
2023-11-11 9:43 AM
Thank you so much for that answer. I'll review the pertinent sections of the rm. My original issue was that I had the BOOT0 pin floating which caused the MCU to execute out of uninitialized RAM the first time I applied power. I was using a current limited power supply that limited damage to the MOSFET and gate driver. I found that I could program the option bits to ignore the BOOT0 pin but that was not the default setting and have since added a pull-down on the BOOT0 pin to fix it so that the MCU can get programmed without damaging the board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.