cancel
Showing results for 
Search instead for 
Did you mean: 

Request for HM01B0 Camera Module Drivers for STM32

Wulfenlied
Associate

Hello,

Hello,

I am seeking either a ready-to-use or partially implemented driver for the  HM01B0 - QVGA SPI Camera Module to use with the NUCLEO-F767ZI board.

My aim is to recreate a project I previously completed with the Portenta H7 on the OpenMV IDE, but this time I want to write the code in C instead of MicroPython.

The goal is to optimize the project, gain a deeper understanding of the hardware, and move further into embedded systems development with something I'm already familiar with.

Any advice or suggestions are also greatly appreciated!

Thank you in advance,
Moustafa

 

0 REPLIES 0