Request for Hardware Reference Design for RTC in STM32C0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-10-08 11:54 PM
I’m having trouble finding a hardware reference design for the RTC on the STM32C0 series (STM32C031C4).
I need guidance on how to properly design the hardware since the STM32C031C4 doesn’t have a VBat pin for battery connection. Could someone please guide me on how to resolve this issue?
Solved! Go to Solution.
- Labels:
-
RTC
-
STM32C0 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-10-09 2:52 AM
Hello @MohanKrish, welcome to ST Community
Quoting from AN5096 "Power supplies and reset sources on STM32G0 Series", "VBAT is the power supply (through a power switch) for RTC, TAMP, low-speed external 32.768 kHz oscillator and backup registers when VDD is not present. VBAT is provided externally through VBAT pin. When this pin is not available on the package, it is internally bonded to VDD/VDDA. "
Although the STM32G0 series has a VBAT pin, the principles of maintaining power to the RTC can be adapted to the STM32C031C4, so, the RTC should be powered by the main VDD supply (it has to be stable and within the recommended operating range).
For backup retention, consider using a supercapacitor with a voltage rating higher than your VDD to maintain the VDD for the required duration during a power outage. (connect it in parallel with VDD so it can charge when VDD is available and discharge when it's lost, also consider using a diode to prevent the capacitor from discharging back into the main power supply)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-10-09 2:52 AM
Hello @MohanKrish, welcome to ST Community
Quoting from AN5096 "Power supplies and reset sources on STM32G0 Series", "VBAT is the power supply (through a power switch) for RTC, TAMP, low-speed external 32.768 kHz oscillator and backup registers when VDD is not present. VBAT is provided externally through VBAT pin. When this pin is not available on the package, it is internally bonded to VDD/VDDA. "
Although the STM32G0 series has a VBAT pin, the principles of maintaining power to the RTC can be adapted to the STM32C031C4, so, the RTC should be powered by the main VDD supply (it has to be stable and within the recommended operating range).
For backup retention, consider using a supercapacitor with a voltage rating higher than your VDD to maintain the VDD for the required duration during a power outage. (connect it in parallel with VDD so it can charge when VDD is available and discharge when it's lost, also consider using a diode to prevent the capacitor from discharging back into the main power supply)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-10-11 1:29 AM
Thank you for your precise reply.