2018-12-28 05:21 AM
Hi sir/ mam,
we are using STM 32f765NIH7 micro controller for our industrial safety project. we just want to know about thermal resistance between case and ambient or please provide max case temperature , so that it's helpful for our derating calculation and SFF calculation
2018-12-28 09:59 PM
Datasheet info not detailed enough?
https://www.st.com/resource/en/datasheet/stm32f765ni.pdf
Page 250
Ageing of the chip typically shrink with higher junction temperature.
2018-12-28 10:09 PM
2018-12-30 11:53 AM
The only other info is page 113 about junction temperature limit to wakl back to max ambiant temperature. (if the application has a plastic case and heating occurs inside...) In an LCD TV, chassis ambiant is typically 60 to 80C.
TA Ambient temperature for 6 suffix version Maximum power dissipation − 40 - 85 °C Low power dissipation(10) − 40 - 105 Ambient temperature for 7 suffix version Maximum power dissipation − 40 - 105 °C Low power dissipation(10) − 40 - 125 TJ Junction temperature range 6 suffix version − 40 - 105 °C 7 suffix version − 40 - 125
I'm not expert in thermal calculations, someone more knowledgeable should answer in more details to the question.
2019-01-10 04:33 AM
Hi @cgedd ,
I would recommend to check with your FAE to get more details about this request.
Khouloud.