2011-11-26 2:13 AM
Hi,
There is a small conceptual issue I wish to report in the STM32F2/F4/L1 headers. Currently the GPIO BSRR register is declared as two separated 16bits registers BSRRL and BSRRH which defeats its purpose of making atomic masked writes possible, that requires a single 32bits access. I recommend redefining it as an union allowing both access modes: volatile union { uint32_t W; struct { uint16_t set; uint16_t clear; } H; } BSRR; This would make possible both simple and masked accesses. Giovanni --- #stm32-headers-rtos