cancel
Showing results for 
Search instead for 
Did you mean: 

received 13byte data on serial port instead of 10 byte

ykn
Senior
/*
 * OTA Command format
 *
 * ________________________________________
 * |     | Packet |     |     |     |     |
 * | SOF | Type   | Len | CMD | CRC | EOF |
 * |_____|________|_____|_____|_____|_____|
 *   1B      1B     2B    1B     4B    1B
 */
typedef struct
{
  uint8_t   sof;
  uint8_t   packet_type;
  uint16_t  data_len;
  uint8_t   cmd;
  uint32_t  crc;
  uint8_t   eof;
}__attribute__((packed)) ETX_OTA_COMMAND_;
 
   
 
    
int send_ota_start(int comport)
{
  uint16_t len;
  ETX_OTA_COMMAND_ *ota_start = (ETX_OTA_COMMAND_*)DATA_BUF;
  int ex = 0;
 
  memset(DATA_BUF, 0, ETX_OTA_PACKET_MAX_SIZE);
 
  ota_start->sof          = ETX_OTA_SOF;
  ota_start->packet_type  = ETX_OTA_PACKET_TYPE_CMD;
  ota_start->data_len     = 1;
  ota_start->cmd          = ETX_OTA_CMD_START;
  ota_start->crc          = 0x00;               //TODO: Add CRC
  ota_start->eof          = ETX_OTA_EOF;
 
  len = sizeof(ETX_OTA_COMMAND_);
 
  //send OTA START
  for(int i = 0; i < len; i++)
  {
    delay(1);
    if( RS232_SendByte(comport, DATA_BUF[i]) )
    {
      //some data missed.
      printf("OTA START : Send Err\n");
      ex = -1;
      break;
    }
  }
 
  if( ex >= 0 )
  {
    if( !is_ack_resp_received( comport ) )
    {
      //Received NACK
      printf("OTA START : NACK\n");
      ex = -1;
    }
  }
  printf("OTA START [ex = %d]\n", ex);
  return ex;
}    
int RS232_SendByte(int comport_number, unsigned char byte)
{
  int n;
 
  if(!WriteFile(Cport[comport_number], &byte, 1, (LPDWORD)((void *)&n), NULL))
  {
    return(1);
  }
 
  if(n<0)  return(1);
 
  return(0);
}

hi,

I am working on FOTA implementation programm. for that i have to send flash to serial.

i have done some code gcc to send data. but instead of 10 byte i have received 13 byte .

below is the function code.

the compiler i used is GCC on windows 64 bit

please guide me where i am wrong

9 REPLIES 9

You'll need to byte pack the structure. Check sizeof()​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Jaroslav JANOS
ST Employee

Hello ykn,

try the following instead:

typedef struct __attribute__((packed)) {
  uint8_t   sof;
  uint8_t   packet_type;
  uint16_t  data_len;
  uint8_t   cmd;
  uint32_t  crc;
  uint8_t   eof;
} ETX_OTA_COMMAND_;

BR,

Jaroslav

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

same output, not working

returning 13 size. what is he correct format

gbm
Principal

Define crc as a vector of four bytes and fill it byte by byte. Looks like packed attribute cannot deal with unaligned data and results in stripping the final padding only, which means IT DOESN'T work (since it's supposed to support vectors of structures correctly).

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Pavel A.
Evangelist III

To my surprise :( the modern GCC documentation for attribute((packed)) does not mention that attribute((packed)) can be applied to a struct as a whole.

Rather, it provides example where packed is applied to a struct member/field, and attribute((aligned)) may be applied to a whole struct or a member/field. And aligned behaves differently on a struct object definition vs. a typedef.

This IMHO is in favor of what @gbm​ advises. Live and learn...

#include <stdint.h>
#include <assert.h>
 
typedef struct __attribute__((packed)) {
	uint8_t   sof;
	uint8_t   packet_type;
	uint16_t  data_len;
	uint8_t   cmd;
	uint32_t  crc;
	uint8_t   eof;
} ETX_OTA_COMMAND_;
 
static_assert(sizeof(ETX_OTA_COMMAND_) == 10);

Compiles without any problems on ARM GNU Toolchain 10.3-2021.10 .

My bad. Looked in a wrong GCC manual section. Your example shows a type attribute, not variable attribute. For types (whole struct) it is legal.