cancel
Showing results for 
Search instead for 
Did you mean: 

Readout unprotect command

lil-vince
Associate II
Posted on August 31, 2009 at 13:59

Readout unprotect command

1 REPLY 1
lil-vince
Associate II
Posted on May 17, 2011 at 13:22

Hi all,

Does the Readout unprotect command always erase the entire Flash even if the Readout protection was not set?

And is the result, the same as the erase entire flash command?

To be short, can we use the Readout unprotect command to erase the entire flash instead of the erase command to simplify the Flash loader program?

Thanks