cancel
Showing results for 
Search instead for 
Did you mean: 

Reading wrong size on an eMMC (THGBMHG6C1LBAIL) 8GBytes (8*8Gb)

Julien M
Associate II
Posted on August 01, 2017 at 10:45

Hi,

I have an 8GB eMMC memory and when I read the capacity I can obtain  (2097152*512)/(1024*1024*1024) = 1 GB0690X00000607kBQAQ.png

What is the limitation of HAL library about the size of an eMMC ? How I can bypass this issue ?

After some research it seems to be I need to read another register on HIGH CAPACITY cards EXT_CSD  and use sector adresse instead of byte address, but why they are not present on the HAL ?

I need to develop by myself all the thing ?

Somebody can help me ?

Thank you so much.

0 REPLIES 0