Solved
Input capture Porblem
Posted on July 31, 2017 at 13:55
Hey
I use stm32f030p4 and i want counting a external frequency (Learning remote ).
I configure timer and interrupts like this
TIM_ICInitStructure.TIM_Channel = TIM_Channel_1;TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;TIM_ICInitStructure.TIM_ICFilter = 0x0;TIM_ICInit(TIM3, &TIM_ICInitStructure);/* Enable the CC2 Interrupt Request */TIM_ITConfig(TIM3, TIM_IT_CC1, ENABLE);/* Enable the TIM1 global Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;NVIC_InitStructure.NVIC_IRQChannelPriority = 0;NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_Init(&NVIC_InitStructure);uint32_t now =0;
void TIM3_IRQHandler(void)
{if(TIM_GetITStatus(TIM3, TIM_IT_CC1) == SET){TIM_ClearITPendingBit(TIM3,TIM_IT_CC1);
now=TIM_GetCapture1(TIM3);
}
}
Interrupt work good but
TIM_GetCapture1(TIM3) is always 0 .
how can i solve this problem?