Reading different CPUID when ever STM32F107 is power cycled.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-13 6:31 PM
Hi ST community,
I am trying to read the CPUID of STM32F107 using the following code snippet. But the problem is each time I power cycle it, I am reading a different CPUID.
I am reading CPUID from address location UID_BASE_ADDRESS(0x1FFFF7E8) for STM32F107.
I am also using same code snippet for STM32F407, and reading CPUID from the address location UID_BASE_ADDRESS(0x1FFF7A10), in this case I am able to read the same
CPUID across power cycles. What might be the problem in case of STM32F107?
#define INDEX_ZERO ((uint8_t) 0)
#define INDEX_ONE ((uint8_t) 1)
#define INDEX_TWO ((uint8_t) 2)
void Get_CPU_UID ( unsigned int * uid_in_buff )
{
unsigned int * UID_ptr = (unsigned int *) UID_BASE_ADDRESS;
if(uid_in_buff != (unsigned int *)RESET)
{
uid_in_buff[INDEX_ZERO] = UID_ptr[INDEX_ZERO];
uid_in_buff[INDEX_ONE] = UID_ptr[INDEX_ONE];
uid_in_buff[INDEX_TWO] = UID_ptr[INDEX_TWO];
}
}
Thank you,
Regards,
Sai
- Labels:
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-13 7:26 PM
Check that your clock settings and flash wait states are valid.