Skip to main content
DGran.3
Associate II
February 3, 2022
Question

Read multiple samples from external ADC via SPI DMA with discontinuous SCK

  • February 3, 2022
  • 1 reply
  • 1062 views

I'm working with a 24-bit external ADC (LTC2512-24) and stm32u5 (NUCLEO).

With the MCU as master, after Data Ready Line (DRL) falling edge from the ADC I need to read 24bits via SPI within 740ns and then have SCK remain quiet until the next DRL falling edge (the quiet is to prevent causing ADC noise).

I have used autonomous mode triggered on DRL falling edge and this works to generate a DMA request and read a sample value, but it only triggers once and reads one ADC sample.

To get it to read in a cycle I have to use the SPI transfer complete ISR to setup a new DMA receive transfer but this means I have to process each sample individually which means I need to wake very frequently. How can I read more samples in one transfer without continuous SCK output?

Could I use DRL to trigger a one-pulse mode timer output with a width equivalent to 24 SCK pulses and use this as my RDY signal for SPI? When RDY is low won't this pause the transfer, so I could then use a large TSIZE to receive many samples?

Is there an easier/better method?

This topic has been closed for replies.

1 reply

DGran.3
DGran.3Author
Associate II
February 7, 2022

Ended up using the RDY method I described above and seems to work ok.