2013-03-28 02:12 AM
Hi,
in the file System_ST32F4xx.c of the ST4Discovery examples, I always find the following 2 lines for the clock configuration (SysClk 168MHz):/* HCLK = SYSCLK / 1*/
RCC->CFGR |= RCC_CFGR_HPRE_DIV1; /* PCLK2 = HCLK / 2*/ RCC->CFGR |= RCC_CFGR_PPRE2_DIV2; /* PCLK1 = HCLK / 4*/ RCC->CFGR |= RCC_CFGR_PPRE1_DIV4; I understand the meaning for the last 4 lines - here SysClk must be devided by 2 or 4, resp., as the APB1 and APB2 frequencies are limited to 84MHz and 42MHz. But concerning the first 2 lines, here the RM 6.3.3(RCC_CFGR) states:Bits 7:4 HPRE: AHB prescaler
Set and cleared by software to control AHB clock division factor. ... 0xxx: system clock not divided 1000: system clock divided by 2 ... So according to this register description, RCC_CFGR_HRPE could be left on its init value of 0. Why is it programmed to the value ''2'' in the ST4Discovery examples? Anyone has any idea?2013-03-28 04:25 AM
I'd guess that they are autogenerated or simply product of copy/paste. Take it as a template for your code where you might potentially want to use a different divider.
> Why is it programmed to the value ''2'' in the ST4Discovery examples?
In my copy of stm32f4xx.h:#define RCC_CFGR_HPRE_DIV1 ((uint32_t)0x00000000) /*!< SYSCLK not divided */
Where do you have ''2'' from? JW2013-03-28 08:30 AM
Thank you for your answer.
The commandRCC->CFGR |= RCC_CFGR_HPRE_DIV1
puts HPRE to ''2'' (as DIV1 is the 2nd bit in this HPRE field).2013-03-28 08:52 AM
No. The C compiler doesn't know about what is written in reference manual.
Check howRCC_CFGR_HPRE_DIV1
is defined in the library files you are including/linking. Chances are, that it's a macro defined as I described above. JW [EDIT] Oh, I now see what's the source of your confusion:#define RCC_CFGR_HPRE_1 ((uint32_t)0x00000020) /*!< Bit 1 */
versus#define RCC_CFGR_HPRE_DIV1 ((uint32_t)0x00000000) /*!< SYSCLK not divided */
Oдна буква и кака�? разница... 😉 JW