cancel
Showing results for 
Search instead for 
Did you mean: 

RADC of STM32G0B1xB/xC/xE

aki49
Associate II

I want to know the value of RADC in "Figure 29. Typical connection diagram using the ADC" of STM32G0B1xB/xC/xE?

Alternatively, I would like to know the maximum value of RADC.

STM32G0 Series

2 REPLIES 2
Sarra.S
ST Employee

Welcome @aki49 to ST Community, 

Please note that the Radc is not constant - it depends on temperature, VDD voltage, usage of Analog switches booster.

In fact, we take into account the Radc value when calculating the Rain Max indicated in the datasheet. 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you for your reply Sarra.S.

How is the Radc value calculated? Or is there a description of the maximum value?