2022-12-11 05:34 AM
Hello everybody.
I use the STM32F746G-DISCO board. I checked all LCD operations using TouchGFX, but at some point, nothing appears on the LCD screen even when I connect USB to the computer.
When connecting using STM32CubeProgrammer, only the phrase "No STM32 target found" appears and it is confirmed that connection is not possible.
I tried connecting by changing the USB, and tried connecting while pressing the reset button, but the result did not change.
What should I do to solve this problem?
Solved! Go to Solution.
2022-12-11 06:19 AM
Check powering jumpers on disco
2022-12-11 06:19 AM
Check powering jumpers on disco
2022-12-11 06:42 AM
not clear:
board + connection was working
or
it is new and never worked ?
2022-12-11 04:10 PM
The board has been working fine for about 3 weeks since I bought it. But since then I have confirmed that it is not connecting.
2022-12-11 04:18 PM
I solved it.
I checked the power jumper and it was badly connected. It was a stupid mistake, but I fixed it thanks to you.