cancel
Showing results for 
Search instead for 
Did you mean: 

question about VDD pin

DAR20_01
Associate II

I'm a beginner and I don't understand the datasheet very well. Can I externally power my STM32 F446RE from the VDD pin (the one opposite E5V in the pinout)?
Sorry for the banality, but I only found info for generic GPIOs.
Dar

1 ACCEPTED SOLUTION

Accepted Solutions

Putting 5V on VDD will kill the chip.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

What board are you referring to?

 


 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Ciao amico.
Mi dispiace. La scheda è la STM32 Nucleo F446RE 
"https://www.st.com/en/evaluation-tools/nucleo-f446re.html" 

TDK
Super User

Download the user manual for the board--it goes into the various power options.

In general, yes, you can apply VDD directly, but ensure you're not backpowering something. The schematic can be downloaded from the board product page. Generally, VDD is powered from the board so providing external power may not do what you want.

If you feel a post has answered your question, please click "Accept as Solution".

Hi my friend,
You're right, I read the datasheet. I can power it from E5V and Vin. My problem is that I've already connected the Murata 24/5 Output to the VDD pin via a PCB track. This avoids damaging the board by powering it externally.
During the design phase, due to the file transfer, we missed this aspect.
Anyway, thanks guys for the quick replies!

DAR20_01
Associate II

So am I doing any harm by powering with 5V into the Vdd? I've already made the connections (on the PCB) I just want to avoid breaking the board now

Putting 5V on VDD will kill the chip.

If you feel a post has answered your question, please click "Accept as Solution".