2017-06-30 5:57 AM
Hello Team,
I have purchased STM32F7 disco board. I want to use CubeMx tool to generate code and modify/use it.
Can I get CubeMx project for STM32F7 discovery board : STM32F769i - DISCO (MB1225B)
Thank you,
Solved! Go to Solution.
2017-06-30 8:40 AM
2017-06-30 6:10 AM
Hi
arror.balaraju
,A set of examples usingSTM32F769NI discovery board are available under the STM32F7 firmware package:
STM32Cube_FW_F7_V1.7.0\Projects\STM32F769I-Discovery
-Nesrine-
2017-06-30 6:13 AM
About using QSPI on STM32F7 a set of example are provided under the STM32F7 firmware package and can be
easily tailored to any other supported device and development board.STM32Cube_FW_F7_V1.7.0\Projects\STM32F769I_EVAL\Examples\QSPI
2017-06-30 6:33 AM
Hello Nesrine,
Thank you for the help. I will use this example to explore QSPI.
I have other question is, can I get CubeMx project for the discovery board: STM32F769i - DISCO (MB1225B).
I want know how the components are configured in STM32CubeMx project. This I will take reference for my development.
Thank you,
2017-06-30 8:40 AM
2017-06-30 8:51 AM
Hello Nesrine,
I am sorry, I could not explain correctly.
I have some knowledge on STM32MxCube. I know how to configure components.
But in case of Discovery board I do not have schematic. If I can get cube project, I can understand which all are components are connected to the host and via which communication they are connected. How LCD is connected? Of course via DSI, that I understood. But how LTDC is controlling ?? Which buffer is used for screen composition ? external SDRAM? how this SDRAM is accessed? via FMS?? DMA?? , why QSPI is used? to execute the code or only to fetch fonts etc.
If I can get the cube project that would be great help
Thank you,
2017-06-30 7:27 PM
schematic is in the user manual.
and also at the board's site
drivers for the components on the board are in the board support package
STM32Cube_FW_F7_V1.7.0/Drivers/BSP/STM32F769I-Discovery
2017-07-04 3:36 AM
Thank you,
I got answer in previous reply. I could not realize it.
2017-10-19 3:18 AM
Hi Nesrine,
there are no example to QSPI on STM32F769I_DISC0 ...I tried to adapter the example on STM32F769I_EVAL changing the GPIO configuration but it still don't work
Do you have a working example?