cancel
Showing results for 
Search instead for 
Did you mean: 

QSPI from Dual to Single flash mode

ROlii.1
Associate

Hello, I tried to start QSPI working on a Single flash mode but have a problem with non readable part config registers (NonVolatile, Volatile and Enhanced Volatile). As I understand when working in Dual Flash mode this registers should write and read in pairs, but I receive this weird data(the screen below). In Single flash mode all registers have only 0x55. The question is:

  1. How to wake up the second chip of external flash memory?
  2. What are the right configurations for Single flash mode?

The microcontroller is STM32H750B-DK and external memory MT25QL512ABB0693W00000Ly4hwQAB.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

The BOARD is STM32H750B-DK, the MCU is STM32H750XBH6

Will come down to initialization code, which you don't show.

The two chips share a common chip select, but the second one is the QSPI BK2 data pins.

You should be able to read a byte if dual mode is disabled, and you use QSPI_FLASH_ID_1

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

The BOARD is STM32H750B-DK, the MCU is STM32H750XBH6

Will come down to initialization code, which you don't show.

The two chips share a common chip select, but the second one is the QSPI BK2 data pins.

You should be able to read a byte if dual mode is disabled, and you use QSPI_FLASH_ID_1

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ROlii.1
Associate

This register read is from dual-flash config. This is the initialization code:

void MX_QUADSPI_Init(void)
{
 
  /* USER CODE BEGIN QUADSPI_Init 0 */
 
  /* USER CODE END QUADSPI_Init 0 */
 
  /* USER CODE BEGIN QUADSPI_Init 1 */
 
  /* USER CODE END QUADSPI_Init 1 */
  hqspi.Instance = QUADSPI;
  hqspi.Init.ClockPrescaler = 1;
  hqspi.Init.FifoThreshold = 1;
  hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
  hqspi.Init.FlashSize = 19;
  hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
  hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
//#ifdef FLASHID
//  hqspi.Init.FlashID = QSPI_FLASH_ID_1;
//#else
    hqspi.Init.FlashID = QSPI_FLASH_ID_1;
//#endif
  hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
  if (HAL_QSPI_Init(&hqspi) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN QUADSPI_Init 2 */
 
  /* USER CODE END QUADSPI_Init 2 */
 
}
 
void HAL_QSPI_MspInit(QSPI_HandleTypeDef* qspiHandle)
{
 
  GPIO_InitTypeDef GPIO_InitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
  if(qspiHandle->Instance==QUADSPI)
  {
  /* USER CODE BEGIN QUADSPI_MspInit 0 */
 
  /* USER CODE END QUADSPI_MspInit 0 */
  /** Initializes the peripherals clock
  */
    PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_QSPI;
    PeriphClkInitStruct.QspiClockSelection = RCC_QSPICLKSOURCE_D1HCLK;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
    {
      Error_Handler();
    }
    /* QUADSPI clock enable */
    __HAL_RCC_QSPI_CLK_ENABLE();
 
    __HAL_RCC_GPIOG_CLK_ENABLE();
    __HAL_RCC_GPIOF_CLK_ENABLE();
    __HAL_RCC_GPIOD_CLK_ENABLE();
    /**QUADSPI GPIO Configuration
    PG6     ------> QUADSPI_BK1_NCS
    PF6     ------> QUADSPI_BK1_IO3
    PF7     ------> QUADSPI_BK1_IO2
    PF10     ------> QUADSPI_CLK
    PF9     ------> QUADSPI_BK1_IO1
    PD11     ------> QUADSPI_BK1_IO0
    */
    GPIO_InitStruct.Pin = GPIO_PIN_6;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;
    HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_10;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
    HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = GPIO_PIN_9;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;
    HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = GPIO_PIN_11;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
    HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
  /* USER CODE BEGIN QUADSPI_MspInit 1 */
    __HAL_RCC_GPIOC_CLK_ENABLE();
    __HAL_RCC_GPIOH_CLK_ENABLE();
    /**QUADSPI GPIO Configuration
    PG9     ------> QUADSPI_BK2_IO2
    PG14     ------> QUADSPI_BK2_IO3
    PF10     ------> QUADSPI_CLK
    PH2     ------> QUADSPI_BK2_IO0
    PH3     ------> QUADSPI_BK2_IO1
    */
    GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_14;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
    HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = GPIO_PIN_10;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
    HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
    HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
 
 
    // Reset the QuadSPI memory interface 
    __HAL_RCC_QSPI_FORCE_RESET();
    __HAL_RCC_QSPI_RELEASE_RESET();
    
        // NVIC configuration for QSPI interrupt
    HAL_NVIC_SetPriority(QUADSPI_IRQn, 0x0F, 0);
    HAL_NVIC_EnableIRQ(QUADSPI_IRQn);
  /* USER CODE END QUADSPI_MspInit 1 */
  }
}