2025-02-04 11:42 PM
hi all,
i was trying to work with stm32u585 microcontroller and an external RAM IS66WVQ2M4DALL , which is a QSPI based RAM can work in 133Mhz.the RAM support DDR based data transfer. Here i am attaching my OSPI configuration
hospi1.Instance = OCTOSPI1;
hospi1.Init.FifoThreshold = 1;
hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_APMEMORY;
hospi1.Init.DeviceSize = 20;
hospi1.Init.ChipSelectHighTime = 1;
hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 2;
hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
hospi1.Init.ChipSelectBoundary = 0;
hospi1.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;
hospi1.Init.MaxTran = 0;
hospi1.Init.Refresh = 320;
if (HAL_OSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
sOspiManagerCfg.ClkPort = 1;
sOspiManagerCfg.DQSPort = 1;
sOspiManagerCfg.NCSPort = 1;
sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}
HAL_OSPI_DLYB_Cfg_Struct.Units = 0;
HAL_OSPI_DLYB_Cfg_Struct.PhaseSel = 0;
if (HAL_OSPI_DLYB_SetConfig(&hospi1, &HAL_OSPI_DLYB_Cfg_Struct) != HAL_OK)
{
Error_Handler();
}here i am confused about selecting hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_APMEMORY;
#define HAL_OSPI_MEMTYPE_MICRON ((uint32_t)0x00000000U) /*!< Micron mode */
#define HAL_OSPI_MEMTYPE_MACRONIX ((uint32_t)OCTOSPI_DCR1_MTYP_0) /*!< Macronix mode */
#define HAL_OSPI_MEMTYPE_APMEMORY ((uint32_t)OCTOSPI_DCR1_MTYP_1) /*!< AP Memory mode */
#define HAL_OSPI_MEMTYPE_MACRONIX_RAM ((uint32_t)(OCTOSPI_DCR1_MTYP_1 | OCTOSPI_DCR1_MTYP_0)) /*!< Macronix RAM mode */
#define HAL_OSPI_MEMTYPE_HYPERBUS ((uint32_t)OCTOSPI_DCR1_MTYP_2) /*!< Hyperbus mode */from some forums its get to know that this is based on the data order D0/D1 or D1/D0 from the datasheet of my memory ship the timing diagram look like
so here what option i need to take. and planning to work with memory mapped mode . here when i tried with read and write my read and write is corrupting can anybody check with my configuration
Solved! Go to Solution.
2025-03-19 10:45 PM
hi
this address mapping for QSPI based ISSI chip uses is supported by ST ,